Need urgent help - P1013 JTAG and Bank 0 access not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need urgent help - P1013 JTAG and Bank 0 access not working

550 Views
amit_khanna
Contributor I

I have a board with P1013 processor and need urgent help resolving issue below.

 

I have setup the BOOT option for LB FCM 8-bit NAND Flash Small page. 

CKSTP_OUT0_N = '1' (4.7K pull-up boot strap)

CKSTP_OUT1_N = '0' (4.7K pull-down boot strap)

ETH_PHY_TXD1 = '0' (4.7K pull-down boot strap)

GPP_READY_P0 = '0' (4.7K pull-down boot strap)

 

When accessing the device via JTAG, I get an error.  See attachment.  Please help me understand why required boot strapping pull-down on CKSTP_OUT1_N is causing error on JTAG.

 

If I remove the pull-down on CKSTP_OUT1_N, I am able to access the device via JTAG.

 

After accessing the JTAG any, we tried to access Bank 0 as we have NAND flash connected to Bank 0.  However, it fails. That is, I don't see any activity on Chip Select 0, Write enable, output enable on FCM interface.  However, when I access Bank 1, i see activity on all the signals.  Please help me understand what setting am I missing to Bank 0 access.

 

Following is how we are configured the registers in regards to FCM/NAND Flash

 

#define CONFIG_NAND_ADDR_BOOT 0xEFF00000

 

   // LAWBAR6 - Local Bus NAND (boot)
   //   bit 8 - 31 = 0xEFF00000 - base addr
   MM_LAWBAR6 = CONFIG_NAND_ADDR_BOOT >> 12;
   
   // LAWAR6
   //   bit 0 = 1 - enable window
   //   bit 7-11 = 00100 - Local Bus
   //   bit 26-31 = 001111 64k - size
   MM_LAWAR6 = 0x8040000f;

 

   // CS0 - NAND Flash (boot)  
   //   BR0 base address at 0xEFF00000, port size 8 bit, FCM
   eLBC_BR0 = 0xf8001001;
   //   OR0 64KB flash size, FCM (large page NAND Flash)
   eLBC_ORf0 = 0xf8000ff7;

 

Regards,

Amit

Original Attachment has been moved to: target-init-fail.txt.zip

Labels (1)
0 Kudos
1 Reply

350 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Amit,

The CKSTP_OUT pin is an output that tell external hardware that the processor is in a checkstop state, it is not used by the debugger, it is recommended with 10K pull up. The pin itself does not cause the reset, a reset will put CKSTP_OUT in high-Z and the recommended pull-up will ensure the signal is negated after the reset sequence is complete.

For bank0 NAND Flash accessing problem, there is problem with BR0 and OR0 registers configuration in your description.

Please refer to the following configuration from CodeWarrior initialization file.

# BR0 base address at 0xEFF00000, port size 8 bit, FCM, ECC checking and generation are disabled

mem [CCSR 0x5000] = 0x[format %x [expr 0xEFF00821 | $ECC_EN]]

if {$ROM_LOC == $FCM_SMALL_PAGE_BOOT_LOC} {

  # boot from fcm small page boot location

  # OR0 64KB flash size, FCM (small page NAND Flash)

    mem [CCSR 0x5004] = 0xFFFF0796

} else {

# boot from fcm large page boot location

# OR0 64KB flash size, FCM (large page NAND Flash)

mem [CCSR 0x5004] = 0xFFFF07AE

}

Please refer to the following BR and OR registers definition, for details please refer to the processor reference user manual.

pastedImage_13.png

Base Registers definition is similar as the above

BA: Base address.

PS:Port Size

Option Register definition is as the following.

pastedImage_14.png

AM: GPCM address mask.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos