Hi,
I can run the following command, then video is displayed correctly.
chromium --no-sandbox /run/media/sda1/video2/BigBuckBunny_640x360_WEBM.html
But as soon as I change the mouse pointer position, chromium crashes :
[1723:1723:1201/144550.721866:ERROR:cursor_loader.cc(114)] Failed to load a platform cursor of type kNull
[1723:1766:1201/144554.130035:ERROR:chrome_browser_main_extra_parts_metrics.cc(226)] crbug.com/1216328: Checking Bluetooth availability started. Please report if there is no report that this ends.
[1723:1766:1201/144554.130292:ERROR:chrome_browser_main_extra_parts_metrics.cc(229)] crbug.com/1216328: Checking Bluetooth availability ended.
[1723:1766:1201/144554.130421:ERROR:chrome_browser_main_extra_parts_metrics.cc(232)] crbug.com/1216328: Checking default browser status started. Please report if there is no report that this ends.
[1723:1766:1201/144554.192241:ERROR:chrome_browser_main_extra_parts_metrics.cc(236)] crbug.com/1216328: Checking default browser status ended.
[ 1160.850453] Alignment trap: not handling instruction f9200791 at [<05b4dd56>]
[ 1160.858265] 8<--- cut here ---
[ 1160.862319] Unhandled fault: alignment exception (0x011) at 0x26ef2474
[ 1160.869079] pgd = afbcda40
[ 1160.871802] [26ef2474] *pgd=1b613831, *pte=2347675f, *ppte=23476c7f
[ 1160.911258] Alignment trap: not handling instruction f9200791 at [<05b4dd56>]
[ 1160.918570] 8<--- cut here ---
[ 1160.921823] Unhandled fault: alignment exception (0x011) at 0x26ef36bc
[ 1160.929033] pgd = afbcda40
[ 1160.932297] [26ef36bc] *pgd=1b613831, *pte=2446675f, *ppte=24466c7f
For the moment I have tested with xwayland and wayland, problem is the same in both configurations. (I have read in i.MX Yocto Project User's Guide that fsl-imx-x11 is not supported anymore.)
MACHINE=imx6qsabresd DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b bld-xwayland-imx6qsabresd
bitbake imx-image-multimedia
MACHINE=imx6qsabresd DISTRO=fsl-imx-wayland source ./imx-setup-release.sh -b bld-wayland-imx6qsabresd
bitbake imx-image-multimedia
Do you know if these configurations are supposed to work correctly with chromium ?
More generally, I am looking for a BSP for i.MX6 as recent as possible, with chromium working on it.
Regards
Hello @Zhiming_Liu ,
Yes, after posting the message, I made a test with hardknott 5.10.72-2.2.2 : this version is working properly.
Do you know if other users had the same kind of problems as me with iMX6 + kirkstone 5.15.32-2.0.0 + chromium ?
Best regards
Fabien
There are currently no related similar issues.
Please put the kernel log and test the video under /home folder.