[iMX93EVK]: Configuring iMX93EVK to act as a USB Mass Storage device.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[iMX93EVK]: Configuring iMX93EVK to act as a USB Mass Storage device.

[iMX93EVK]: Configuring iMX93EVK to act as a USB Mass Storage device.

This article is rather short that only mentions the script that is needed to make an iMX93EVK act as a USB mass storage device so that whenever you connect your iMX device to a windows/linux system via USB, it should get enumerated something like a usb drive. 

The storage that is used in this example is mmc so the expectation is that you have inserted a mmc card in the slot.

Below is the script:-


#!/bin/sh

 

# This composite gadget include function:

# - MASS STORAGE

 

 

#

# Exit status is 0 for PASS, nonzero for FAIL

#

STATUS=0

 

# Check if there is udc available, if not, return fail

UDC_DIR=/sys/class/udc

if test "$(ls -A "$UDC_DIR")"; then

echo "The available udc:"

for entry in "$UDC_DIR"/*

do

echo "$entry"

done

else

STATUS=1

echo "No udc available!"

exit $STATUS;

fi

 

id=1;

udc_name=ci_hdrc.0

#back_file=/dev/mmcblk1

back_file=/tmp/lun0.img

 

mkdir /sys/kernel/config/usb_gadget/g$id

cd /sys/kernel/config/usb_gadget/g$id

 

# Use NXP VID, i.MX8QXP PID

echo 0x1fc9 > idVendor

echo 0x12cf > idProduct

 

mkdir strings/0x409

echo 123456ABCDEF > strings/0x409/serialnumber

echo NXP > strings/0x409/manufacturer

echo "NXP iMX USB Composite Gadget" > strings/0x409/product

 

mkdir configs/c.1

mkdir configs/c.1/strings/0x409

 

echo 5 > configs/c.1/MaxPower

echo 0xc0 > configs/c.1/bmAttributes

 

mkdir functions/mass_storage.1

echo $back_file > functions/mass_storage.1/lun.0/file

ln -s functions/mass_storage.1 configs/c.1/

 

echo $udc_name > UDC



First execute the script.
After that insert the g_mass_storage module in the kernel by executing :-

modprobe g_mass_storage file=/dev/mmcblk1 removable=1


In the dmesg output, you will see something like below:-

 

gauravsharma7_0-1714041731840.png


After that you can connect a C type USB cable to the USB1 port of imx93evk and the other end to any USB ports of a laptop. The moment it is connected, you would be able to see a USB drive similar to what you get when we connect a pen-drive. 


Comments

The simple following three lines work with i.MX93 evk.

modprobe usbcore
modprobe usb_f_mass_storage
modprobe g_mass_storage file=/dev/mmcblk0 removable=1

@hustdage yeah I didn't try via inserting usbcore and usb_f_mass_storage module. I will give it a try. Thanks for the info  

No ratings
Version history
Last update:
3 weeks ago
Updated by: