TDA8024TT VDD question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TDA8024TT VDD question

Jump to solution
1,050 Views
jackylu
Contributor II

Hi,

Would you please help to check as below?

(1) any restriction for the power sequence of VDD(supply voltage 3.3V) and VDDP(DC-DC supply voltage 5V) (2) Will TDA8024TT be broken when VDD is 0V & VDDP is 5V?

Labels (1)
Tags (1)
1 Solution
828 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi, jacky

(1) any restriction for the power sequence of VDD(supply voltage 3.3V) and VDDP(DC-DC supply voltage 5V)

No, there is no restriction. TDA8024 and the microcontroller must use the same VDD supply.

See applicaton diagram in TDA8024 datasheet, please! page 24.

(2) Will TDA8024TT be broken when VDD is 0V & VDDP is 5V?

If VDD is 0v, TDA8024TT can't communicate with microcontorller.
because VDD is for Host I/O, even TDA8024TT's reset pin will be low level,
it means TDA8024TT couldn't work.

Have a nice day!

TIC weidong sun

View solution in original post

2 Replies
829 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi, jacky

(1) any restriction for the power sequence of VDD(supply voltage 3.3V) and VDDP(DC-DC supply voltage 5V)

No, there is no restriction. TDA8024 and the microcontroller must use the same VDD supply.

See applicaton diagram in TDA8024 datasheet, please! page 24.

(2) Will TDA8024TT be broken when VDD is 0V & VDDP is 5V?

If VDD is 0v, TDA8024TT can't communicate with microcontorller.
because VDD is for Host I/O, even TDA8024TT's reset pin will be low level,
it means TDA8024TT couldn't work.

Have a nice day!

TIC weidong sun

828 Views
jackylu
Contributor II

Dear Sir,

Good day,

My customer wants to know TDA8024TT/C1 Tj operating maximum temperature.

Do yo have this information?

Thanks

 

0 Kudos