SDK Release data tables

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK Release data tables

PetrKraus
NXP Employee
NXP Employee
0 0 957

SDK Release data tables are outputs of the SDK Generator core. These tables are actually YML files, which are inputs to next phases of the SDK generation process, like the SDK manifest generation, SDK release deployment data file generation, CMSIS pack generation and the Package Builder. The data tables are included into the SDK release superset.

Example: SDK release 9

Superset z the latest RC: https://bitbucket.sw.nxp.com/projects/MCUCORE/repos/mcu-kex/browse?at=refs%2Ftags%2FREL_2.5.0_REL9_R...

Device datatable files: ‘devices/<short_name>/<short_name>.yml

Boafrd datatable files (boards and kits): ‘boards/<board_name>/<board_name>.yml

Relations between boards and kits and additional information about kits: boards/board_kit_map.yml