I'm looking for a vacuum pressure sensor to control a process that operates at -2kPa from ambient atmosphere.
The temperature operating range is from +10 to +50C.
I'm looking for accuracy equal or better than 5%.
Hello Marc,
For your application, the best sensor will be the:
Just in case that you can be interested in a higher pressure range, please see below:
I hope this information can be helpful.
Have a great day,
Paulina
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
i will go with MPXV7002, thanks a lot lisettelozano mcdvoice